LTE TDD

Carrier Aggregation (CA) Config

For Waveform Playback (ARB) capability.

Sets the predefined carrier configuration. This button is shown when an uplink carrier is selected in the vertical tabs of the upper pane.

SCPI Command

[:SOURce]:RADio:LTETdd:WAVeform[:ARB]:CCARrier<n>:ULINk:CONFig:CAGGregation <string>

SCPI Example

:RAD:LTET:WAV:CCAR:ULIN:CONF:CAGG "Config:B10M,Modulation:QPSK"

Notes

Set only

<string>: "name:value,name:value,…"

State Saved

No

Preset

Refer to the element definition of the data part below.

Range

Refer to the element definition of the data part below.

Initial S/W Revision

A.14.00

Element definition of the data part. The preset value is basically the same as the default value of each setting definition.

Settings

Symbols in the data part

Values in the data part

Preset values

Carrier Aggregation Config

CAConfig

CC10M|CC15M|CC20M|CC10MCC10M|CC10MCC20M|CC15MCC15M|CC20MCC20M

CC10M

Modulation

Modulation

QPSK|QAM16|QAM64|QAM256

QPSK

Carrier Aggregation Config

Sets the carrier configuration type of carrier aggregation.

SCPI Command

NA

SCPI Example

–

Notes

No SCPI, GUI only, Read and Write

State Saved

No

Preset

1 Carrier: 10 MHz

Range

1 Carrier: 10 MHz | 1 Carrier: 15 MHz | 1 Carrier: 20 MHz | 2 Carriers: 10 MHz + 10 MHz | 2 Carriers: 10 MHz + 20 MHz | 2 Carriers: 15 MHz + 15 MHz | 2 Carriers: 20 MHz + 20 MHz

Initial S/W Revision

A.14.00

Modulation

Sets Modulation type for full filled configuration.

SCPI Command

–

SCPI Example

–

Notes

No SCPI, GUI only, Read and Write

State Saved

No

Preset

QPSK

Range

QPSK | 16QAM | 64QAM | 256QAM

Initial S/W Revision

A.14.00

Modified S/W Revision

A.19.00 - Added 256QAM

Carrier Uplink Real-Time

Welcome to LTE TDD